Create a checkbox that shows or hides the clock
    Create a checkbox dynamically linked with a user-specific variable that shows or hides the clock.
- Create the checkbox:- InProject view, right-clickMainWindow (type)and select .
- Hover-over the checkbox, select, and enter ShowClockCheckBox. ShowClockCheckBox.
 
- Configure the checkbox:- InProperties, create a dynamic link betweenActiveand .For more information about dynamic links, see Create dynamic links.
- SetTexttoShow clock.
 
Provide Feedback