Develop a persistent setting specific to a user
    Create a checkbox that shows or hides a clock label, which state is persistent based on the currently logged in user.
Application example

     NOTE: 
    
Download a sample project:
 UserSpecificPersistentSetting.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

Select  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback