Configure idle timeout for a page
    If you want a timeout to apply only to a specific page or panel, you can use a NetLogic to configure an idle timeout. Idle timeouts configured using a NetLogic do not apply to the entire project.
- Select.Template Libraries
- InTemplate Libraries, selectScripts.
- UnderComponents, dragIdle Timeoutdirectly into the start window, such asMainWindow (type), inProject view.
- InLibraries, selectClose.
- WithIdleTimeoutLogicselected, inProperties, inEnabled, selectTrueto enable NetLogic. EnablingIdleTimeoutLogicenables the timeout by default.
- InDuration, enter the time before the timeout occurs.
- InProject view, expandIdleTimoutLogicand then selectOnTimeout.
- InPropertiesafterOnTimeout, select. 
- In the browser, expandCommands, expand the type of command, and then select the command that will be executed when the timeout event is triggered.
- ChooseSelect.
page timeout
    
Provide Feedback