Configure idle Timeout
    You can configure a timeout when there is a lack of user activity in the 
FactoryTalk Optix
. A timeout can trigger any custom event. To configure a timeout, the application must have interactive graphic objects. At runtime, inactivity includes a lack of cursor movements, keyboard actions, and user interactions.
You can configure an idle timeout for either a specific page or an entire session.
timeout
idle
idle timeout
    
Provide Feedback