Configure a local library
    Configure a custom local library to store templates of objects and variables.
     TIP: 
    To use a custom local library on another computer, copy the folder with the library name from  to the same location on another computer. Alternatively, you can use remote libraries. See Configure a remote library.
C:\Users\
UserName
\Documents\Rockwell Automation\FactoryTalk Optix\Libraries- From the main toolbar, select.Template Libraries
- InTemplate Libraries, selectand select New library. New library.
- (optional) Enter a name for the library.TIP: In order to use version control, FactoryTalk Optix library names and repository names must match. The library and repository names must contain only alpha numeric characters, numerals, periods, dashes, and underscores.
New library appears in 
Template Libraries
.- Add templates to your library. See Create a template.
local library
local
    
Provide Feedback