Commit a library
    Commit changes to a local or remote library to save changes on the local computer only. Committed changes are not backed up (or pushed) to a remote repository.
Prerequisites
- To commit a library
- From the main toolbar, select.Template Libraries
- Select Commit. Commit.
- Enter a meaningful commit message.
- SelectOK.
A new version of the library is saved on the local computer.
commit
    
Provide Feedback