Configure a change event
    Trigger methods if the value of a variable or object property changes.
     TIP: 
    If you use a controller tag in a change event, the tag always updates at runtime, even if the 
FactoryTalk Optix Application
 does not display the tag value.- InProject view, select an object or a variable.
- InProperties, right-click a variable or a property and select .TIP: If needed, selectto add a variable. 
- InEvents, next toVariableChanged, select. 
- Select a method:- For global methods, expandCommands.
- For local methods, expand the nodes that expose methods (for example, aDataGridnode exposes aRefreshmethod), or expand the node related to a specific NetLogic.
 
- (optional) If the method requires arguments, expand the method and set arguments.
change event
    
Provide Feedback