- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
View variables
View variables in
FactoryTalk Optix Studio
from either Project view
or Properties
.- View variables from either:
- Projectview. Navigate to the folder containing the variables. TheUIfolder cannot contain variables.
- Properties. Select an object, type, or variable inProjectviewor select and object in the editor. The variables or properties for the selected item appear inProperties.
Provide Feedback