MELSEC Q tag

BrowseName
MelsecQTag
SuperType
Tag(Tag)

Properties

Name
BrowseName
DataType
Description
Memory area
MemoryArea
Decode of memory location contents mode.
Maximum length
MaximumLength
(string data only) Maximum number of characters in the string.
Device number
NumDevice
Address in the memory location in which to read/write the tags.
Bit offset
BitOffset
Encoding
Encoding
Decode of memory location contents mode.
Array update mode
ArrayUpdateMode
(Inherited from Tag)
Original data type
OriginalDataType
(Inherited from Tag)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.