Develop an archives manager

Develop an archives manager

Use the preconfigured Zip Unzip NetLogic to create, extract, and password-protect ZIP archives.
Example application
TIP:
You can download a sample project from:
ExampleApplication-ArchivesManager.zip
Prerequisites
  1. To develop the project
  2. Save the project.
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal