Configuration - Supplemental Power Tap View
The Supplemental Power Tap view lets you enable and disable warnings that are related
to switched power.
Supplemental Power Tap View

Warning | Description |
|---|---|
Switched power voltage | Enables a warning when the switched power voltage exceeds the working limit. Default is unchecked and a warning is not sent. Select to enable. |
Switched power over current | Enables a warning when the current for the switched power exceeds its design working limit. If disabled, a warning is not indicated even if the current for the switched power exceeds its design working limit. Select to enable. |
Provide Feedback