Configuration - Port Configuration View

Use the Port Configuration view to view and configure port properties. The settings define how data is sent and received between the port and the attached device. The values are only displayed when the gateway is online.
Power Tap Port Configuration View
Power Tap Port Configuration View
Parameters
Description
Port
Displays the port data is being sent through.
Enable
Displays whether the port is enabled.
Link Status
Displays the port status.
Auto-Negotiate
Enables Auto-Negotiate to enable the device to negotiate the port’s speed and duplex automatically.
Speed Selected
Displays the port’s selected speed if Auto-Negotiate is unchecked.
Current
Displays the port’s current speed.
Selected duplex
Displays the port’s selected duplex if Auto-Negotiate is unchecked.
Current
Displays how much current is allocated to the port.
Port diagnostics
Opens the Port Diagnostic dialog.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal