Configuration - Network View

Use the Network view to view network information.
This information is only available when online, and there is no communication error in the device profile.
Gateway Network View
Gateway Network View
Parameter
Description
Network topology
Displays the current network topology as either:
  • Linear/Star
  • Ring
Network status
Displays the current network status as:
  • Normal
  • Ring Fault
  • Unexpected Loop Detected
Refresh
Retrieves the latest information from the device and displays it in the Network view.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal