Configuration - Gateway View

The Gateway view lets you enable and disable warnings and define the auto addressing method of the
EtherNet/IP
In-cabinet network end nodes.
Gateway View
Gateway View
Warning
Description
Network power voltage
Enables a warning that network power is nearing the working limit.
Default is unchecked. Select to enable.
Network power over current
Enables a warning that current for the network power is nearing the working limit.
If disabled, a warning is not indicated even if current for the network power exceeds its working limit.
Default is unchecked and a warning is not sent. Select to enable.
Switched power voltage
Enables a warning that switched power voltage is nearing the working limit.
Default is unchecked and a warning is not sent. Select to enable.
Switched power over current
Enables a warning that current for the switched power is nearing the working limit.
If disabled, a warning is not indicated even if current for the switched power exceeds its design working limit.
Reference Topology warning
Enable a warning if the reference topology does not match the actual hardware.
If disabled, a warning is not indicated even if Commissioning Object indicates warnings.
Default is unchecked and a warning is not sent. Select to enable.
Devices auto address method
Defines the device addressing method when the device is not addressed by using the reference topology.
Values allowed:
  • Disabled
  • Next available IP address
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal