800F-INT Push Button Communication Interface Modules
800F communication interface modules connect the push buttons
to the system and enhance 800F In-cabinet input devices for electrical control and
switching. 800F communication interface modules are available as non-illuminated or
illuminated and can be snap-fit to 800F-ALP and 800F-ALM latches.
Provide Feedback