Edit a zone
Edit the properties of a zone to specify a name, description, and enable security settings.
- From the navigation bar, select either:
- Canvasand then select a zone.
- Zonesand then, next to the zone, select.
TIP: You can also selectOverviewand then select a zone from the list.
- Make edits toZONE PROPERTIES.For more information, see Zone properties.
Add devices to the zone. See Devices.
Provide Feedback