Zone properties
Use zone properties to define the policy settings to apply to devices that are assigned to this zone.
General
The settings in this area differentiate this zone from other zones.
Property | Description |
|---|---|
Name | The name for the zone. |
Description | A description for the zone. |
CIP Security
The settings in this area relate to how the devices in the zone communicate with other devices.
Property | Description |
|---|---|
Enable CIP Security | Enable CIP Security options for the zone. When selected, additional configuration options are available. Non- CIP Security capable devices can be added to a zone with CIP Security enabled. These devices will have an information icon displayed stating Incompatible with zone configuration . These devices will not receive CIP Security policy themselves, but devices in this zone that are CIP Security capable will add the IP address of the non-CIP Security capable device to their Trusted IP list so that communication between the devices can occur. |
Authentication Method | Select which method the devices use to authenticate.
Non- CIP Security capable devices do not use any authentication method. If non-CIP Security capable devices are present in a zone, an information message displays stating incompatible devices in zone when Certificate or Pre-shared Key is selected. |
I/O Data Security | Select the type of security check to perform on the input and output data.
Non- CIP Security capable devices do not use any I/O Data Security method. If non-CIP Security capable devices are present in a zone, an information message displays stating incompatible devices in zone when I/O Data Security is selected. |
Messaging Security | Select the type of security check to perform on messages received by devices in the zone.
Non- CIP Security capable devices do not use any Messaging Security and cannot provide data integrity checking. If non-CIP Security capable devices are present in a zone, an information message displays stating incompatible devices in zone when Messaging Security is selected. |
DIsable port HTTP (80) | Select to disable communication over port 80. |
Property | Description |
|---|---|
Inbound CIP Bridging to the backplane |
|
Outbound CIP Bridging from the backplane |
|
OPC UA
Zones and conduits follow these non-editable
OPC UA security policy
settings:
- OPC UAclients trustOPC UAservers
- OPC UAservers do not trustOPC UAservers
- OPC UAclients do not trustOPC UAclients
Provide Feedback