Add a zone
Add zones to establish areas of security policy. Devices assigned to a zone trust each other.
- From the navigation bar, select either:
- Canvasand then select .
- Zonesand then selectnext to
ZONES.TIP: You can also selectOverviewand then selectAddfrom the toolbar.
- Make edits toZONE PROPERTIES.For more information, see Zone properties.
Add devices to the zone. See Devices.
Provide Feedback