Device properties
Use device properties to define the device information, security, and network settings for a device.
Device properties defined using the electronic data sheet (EDS) for the device cannot be modified. A device can have one or more ports that are added to the policy model.
Some of the following properties may be read-only for:
- The devices added to the Onboarding Area by Automatic Policy Deployment.
- The devices that are not added to a secure zone.
Device
Property | Description |
|---|---|
Device Name | The name of the device. The name is required and must be unique. Generic devices are automatically named Device . Devices selected by catalog number or discovered are already named.<number> |
Description | An optional description for the device. The description of generic devices is empty by default. Devices selected by catalog number or discovered may have an existing description. |
Catalog number | If defined using device discovery, the catalog number cannot be changed. Otherwise, choose a catalog number from the list. Choosing a Rockwell Automation catalog number automatically completes the Vendor information.A device without a catalog number is listed as a Generic Device . |
Vendor | The name of the device's vendor. If a Rockwell Automation /Allen-Bradley catalog number was provided, this setting is completed by default and cannot be modified. |
Firmware Revision | The firmware revision number of a device. Required to enable CIP Security for a device.This setting is required to apply CIP Security settings to the device ports. FactoryTalk Policy Manager automatically assigns the latest firmware revision to devices added using a catalog number or using Discovery . |
CIP Security capable | Identifies whether a device can use the security settings of the zone. Select to configure additional CIP Security settings for a generic device.The Catalog Number and firmware revision determine the CIP Security capability of a device automatically. |
Property | Description |
|---|---|
Disable CIP Bridging through USB | When selected, it disables inbound and outbound CIP Bridging through the USB port. When cleared, it enables inbound traffic through the USB port. Outbound traffic is enabled if the device supports it. This setting is only available for the devices with the Capable property enabled. The available options may be restricted by Global Settings. |
Property | Description |
|---|---|
Port name and number | The name and number of ports available on the device. Select ![]() For more information, see Port properties. |
TIP:
For generic devices, you can manually add ports as needed by selecting
+
next to Ports
.For
CompactLogix
5380 Controllers and Compact GuardLogix
5380 Controllers that operate in dual mode, you cannot add Port 2
.UA Client
Item | Description |
|---|---|
Name | OPC UA client name.
TIP:
The default
UA Client tab title changes if you change the OPC UA client name. |
IP Address | IP address of the OPC UA client. |
Item | Description |
|---|---|
Zone | The zone that the OPC UA client is assigned to. |
Item | Description |
|---|---|
Export | Exports the OPC UA client certificate. |
Import | Imports the OPC UA client certificate. |
Item | Description |
|---|---|
Sharing identity with the server | OPC UA client shares its identity with the OPC UA server identity. The identity includes the PKI certificate, username, and password. |
UA Server
Item | Description |
|---|---|
Name | OPC UA server name.
TIP:
The default
UA Server tab title changes if you change the OPC UA server name. |
Server URI | Non-editable OPC UA server URI based on the OPC UA server certificate. |
Server URL | The URL of the OPC UA server endpoint. |
Endpoint | List of endpoints with the Sign & Encrypt security policy mode or stricter. For more information, see OPC UA security policy. Select Refresh to refresh the list. |
Endpoint Encryption to use for Deployment | Encryption algorithm for the OPC UA server endpoint to use for deployment.
TIP:
The encryption algorithm may change if you specify a different endpoint in
Server URL . |
Item | Description |
|---|---|
Zone | The zone that the OPC UA server is assigned to. |
Item | Description |
|---|---|
Anonymous | Log on as an anonymous user to the OPC UA server. |
Username | The user name to log on to the OPC UA server. |
Password | The password to log on to the OPC UA server. |
Show Password | Shows the password. |
Item | Description |
|---|---|
Import | Imports the OPC UA server certificate. |
Item | Description |
|---|---|
Verify | Verifies connection to the OPC UA server. |
Sharing identity with the client | OPC UA server shares its identity with the OPC UA client identity. The identity includes the PKI certificate, username, and password. |
Provide Feedback