OPC UA security policy
Manage connections between
OPC UA
servers, OPC UA
clients, and other components of your system policy model.For more information about
OPC UA
, refer to Unified Architecture - OPC Foundation.OPC UA servers
OPC UA
servers
In
FactoryTalk Policy Manager
, OPC UA
servers are device types, which you can add to the policy model and use as conduit endpoints. You can also import certificates of OPC UA
servers. The certificates are exported to
C:\ProgramData\Rockwell Automation\FactoryTalk System Services\OPC UA Deployments
OPC UA
servers support these authentication methods:
- Certificate
- Authenticate with an X.509 certificate granted by a trusted certificate authority.
- Username and password
- Authenticate with a username and password or as an anonymous user.
Message security mode | Security policy | Security level |
|---|---|---|
None | None- None | Low security |
Sign | Basic128Rsa15 | |
Sign & Encrypt | Basic128Rsa15 | |
Sign | Basic256 | |
Sign & Encrypt | Basic256 | |
Sign | Aes128Sha256RsaOaep | Medium security |
Sign & Encrypt | Aes128Sha256RsaOaep | |
Sign | Basic256Sha256 | Hight security |
Sign & Encrypt | Basic256Sha256 | |
Sign | Aes256Sha256RsaPss | |
Sign & Encrypt | Aes256Sha256RsaPss |
TIP:
Rockwell Automation
recommends setting message security mode to Sign & Encrypt.Each
OPC UA
server has its own trust list and admin list. If you add an OPC UA
server to a zone for the first time and deploy the policy model configuration, the zone trust list and admin list overwrites the OPC UA
server trust list and admin list. Consecutive deployments merge the OPC UA
server and zone trust lists and admin lists.For more information about
OPC UA
server properties, see Device properties.OPC UA clients
OPC UA
clients
In
FactoryTalk Policy Manager
, you can add OPC UA
clients to the policy model and use as them conduit endpoints. You can also import and export certificates of OPC UA
clients. The certificates are exported to
C:\ProgramData\Rockwell Automation\FactoryTalk System Services\OPC UA Deployments
IMPORTANT:
If you export
OPC UA
certificates or CSRs from an OPC UA
device and the security policy model contains both a certificate and a CSR, only the certificate is exported.
OPC UA
clients may support these authentication methods:
- Certificate
- Authenticate with an X.509 certificate granted by a trusted certificate authority.
- Username and password
- Authenticate with a username and password or as an anonymous user.
OPC UA security policy in zones and conduits
OPC UA security policy
in zones and conduitsZones and conduits follow these non-editable
OPC UA security policy
settings:
- OPC UAclients trustOPC UAservers
- OPC UAservers do not trustOPC UAservers
- OPC UAclients do not trustOPC UAclients
Conduits with OPC UA endpoints
OPC UA
endpointsWith
OPC UA
endpoints, you can create these conduits:
Endpoint 1 | Endpoint 2 |
|---|---|
Zone | Zone |
Zone | OPC UA server |
Zone | OPC UA client |
Zone | Range |
OPC UA client | OPC UA server |
Conduits must follow these rules:
- Conduits cannot be duplicated, each combination of endpoints must be unique.
- One of the endpoints must beCIP SecurityorOPC UA security policycapable.
- If one endpoint is a zone, the other endpoint cannot be a device within that zone.
- Devices not assigned to any zone or onboarding devices cannot be used as endpoints.
Compatibility
OPC UA security policy
features work with these Rockwell Automation
product families:
- ControlLogix®5580 controllers firmware revision 36.00 or laterTIP: 1756-L81E and 1756-L81EK controllers are not supported.
- GuardLogix®5580 controllers firmware revision 36.00 or laterTIP: 1756-L81ES and 1756-L81ESK controllers are not supported.
- CompactLogix™5380 controllers firmware revision 36.00 or later
- Compact GuardLogix®5380 controllers firmware revision 36.00 or later
- ControlLogix®Process controllers firmware revision 36.00 or laterTIP: 1756-L81E and 1756-L81EK controllers are not supported.
- CompactLogix™Process controllers firmware revision 36.00 or later
- FactoryTalk® Logix Echoversion 36.00 or later
Provide Feedback