- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
CODESYS Tag
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Symbol name | SymbolName | Tag name. | |
Maximum length | MaximumLength | (string data only) Maximum number of characters in the string. | |
Encoding | Encoding | Decode of memory location contents mode. | |
Start array index | StartArrayIndex | ||
Array update mode | ArrayUpdateMode | (Inherited from Tag) | |
Original data type | OriginalDataType | (Inherited from Tag) |
Provide Feedback