Edit a data source
Edit a data source to modify the settings.
TIP:
Models using the edited data source automatically update to reflect the changes. Redeploy applications consuming the impacted models to reflect the modifications done to the data source.
To edit a data source
- SelectData Flow>Data Sources.
- (optional) FromConfigure Data Sources, filter the list of data sources.
- SelectEdit
for the required data source.
- FromConfigure Data Source, modify the settings for the data source.
- SelectSaveto edit the data source.
Provide Feedback