Ptxx Diagnostics parameters

Ptxx Diagnostics
includes these parameters:
Parameter
Description
Value
Short circuit fault
Shows whether an output short circuit or over-current fault is present on the point.
  • None
  • Present
Last fault timestamp for short circuit fault
Shows the timestamp of the last output short circuit or over-current fault in YYYY-MM-DD-HH:mm:SS_mmm (UTC-00:00) format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
  • UTC-00:00 = Time zone
A valid time or
None
if there is no recorded event time.
No load fault
Shows whether a no load fault is present on the channel.
No load faults occur when a signal wire is disconnected from the output device terminal channel or the Removable Terminal Block (RTB) is removed from the device.
  • None
  • Present
Last fault timestamp for no load fault
Shows the timestamp of the last no load fault in YYYY-MM-DD-HH:mm:SS.mmm (UTC-00:00) format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
  • UTC-00:00 = Time zone
A valid time or
None
if there is no recorded event time.
Field power
Shows whether field power is present on the point.
  • None
  • Present
Field power on timestamp
Shows the timestamp of the last time field power turned on in YYYY-MM-DD-HH:mm:SS_mmm (UTC-00:00) format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
  • UTC-00:00 = Time zone
A valid time or
None
if there is no recorded event time.
Field power off timestamp
Shows the timestamp of the last time field power turned off in YYYY-MM-DD-HH:mm:SS_mmm (UTC-00:00) format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
  • UTC-00:00 = Time zone
A valid time or
None
if there is no recorded event time.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal