Loading
CASE STUDY | OIL & GAS
Recent ActivityRecent Activity

From Packaged Power to Operational Value

EPIC Industrial delivers integrated e-house solutions that simplify deployment and optimize costs for midstream oil and gas operations.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
epic industrial oil gas industry packaged power solutions
epic-industrial-logo

EPIC Industrial Technologies is a leading provider of turnkey electrical, power, instrumentation and controls solutions for the oil and gas, petrochemical, and heavy industrial sectors. Through integrated engineering, procurement, fabrication, and construction services, the company helps customers design, build, and deploy complex industrial infrastructure with efficiency, reliability, and project predictability. As a member of the Rockwell Automation PartnerNetwork™ program, EPIC pairs deep industry expertise with advanced automation and power technologies to deliver scalable, high-performance solutions that support customers throughout the project lifecycle.

Josh Wilkerson
EPIC Industrial Owner, President, and Director
Challenge

  • Growing demand for compressor station and pipeline infrastructure
  • Aggressive schedules for greenfield and expansion projects
  • Remote operating environments with limited skilled labor
  • Need for repeatable, standardized electrical architecture
  • Pressure to lower project costs without compromising reliability
Solution

  • Intelligent Packaged Power™ Solutions
  • PowerFlex® 6000T Variable Frequency Drives
  • Synchronous Transfer Control
  • CENTERLINE® Motor Control Centers
Result

  • Accelerated compressor station deployment through factory-tested e-house solutions
  • Lower capital costs through optimized synchronous transfer architectures
  • Reduced on-site construction and commissioning in remote locations
  • Improved reliability and availability for critical compression assets
  • Standardized electrical designs that scale across midstream facilities

As midstream oil and gas operators expand compression, transportation, and processing infrastructure, they face a common challenge: delivering reliable electrical systems on aggressive schedules, often in remote locations where skilled labor and specialized expertise are limited.

EPIC Industrial Technologies and Rockwell Automation are advancing a more standardized approach to electrical infrastructure delivery. Together, they provide integrated e-house solutions that package critical power and control equipment into factory-tested systems, enabling faster project execution, simplified deployment, and reliable operation.

Challenge

Midstream oil and gas facilities require significant electrical infrastructure to power compressors, pumps, and other critical equipment. Traditional field-built installations can require extensive on-site construction, coordination among multiple suppliers, and lengthy commissioning activities.

Many projects are also in remote areas, creating additional challenges related to labor availability, logistics, and startup support.

At the same time, operators are under pressure to control capital spending while maintaining uptime and operational performance. Customers increasingly need standardized, repeatable electrical solutions that can be engineered efficiently, deployed quickly, and support long-term operational reliability.

Solution

EPIC addresses these challenges through modular e-house solutions that package power distribution, motor control, medium-voltage drives, and automation technologies into a single factory-tested system. Built on technologies from the Rockwell Automation Intelligent Packaged Power portfolio, these standardized designs simplify engineering, reduce project risk, and support repeatable deployment across midstream facilities.

EPIC’s engineering and integration approach has been successfully deployed across multiple midstream projects in Texas and New Mexico. At the center of many of these installations is the PowerFlex® 6000T medium-voltage drive. The drive’s proven performance and support for advanced capabilities such as synchronous transfer make it well suited for midstream oil and gas applications. The PowerFlex 6000T enables flexible, cost-effective electrical architecture while maximizing available space within the e-house. Rockwell Automation has also developed additional drive ratings to meet EPIC’s customers’ specifications, helping EPIC win the business.

EPIC’s partnership with Rockwell Automation extends beyond technology. With specialized training on Rockwell Automation medium-voltage solutions, EPIC provides local startup, commissioning, and technical support, helping customers bring critical compression assets online faster and with greater confidence.

Optimizing Cost and Performance Through Synchronous Transfer

As operators look for opportunities to improve project economics without compromising reliability, many EPIC solutions incorporate synchronous transfer control with PowerFlex 6000T drives. Rather than deploying a dedicated medium-voltage drive for every motor, synchronous transfer enables a single drive to start and operate multiple motors as process conditions require.

Compared to traditional one-drive-per-motor architectures, synchronous transfer can lower capital costs by reducing the number of drives required while decreasing electrical-room footprint, cooling requirements, maintenance costs, and spare-parts inventory. It also minimizes mechanical and electrical stress during motor starts, supporting greater reliability, equipment availability, and long-term system performance.

The solution extends beyond medium-voltage drives to include other technologies from the Rockwell Automation Intelligent Packaged Power™ portfolio, including CENTERLINE® 2100 low-voltage motor control centers. This modular approach gives EPIC a repeatable framework for delivering electrical infrastructure while allowing solutions to be tailored to each customer's requirements.

"By combining EPIC's integration expertise with innovative power solutions from Rockwell Automation, we're helping customers bring critical assets online faster and more efficiently," said Josh Wilkerson, EPIC Industrial Owner, President, and Director.

epic industrial sync transfer graphic
Result

By combining standardized e-house designs with a repeatable integration approach, EPIC enables customers to accelerate deployment of compressor stations and other midstream infrastructure. Factory-tested systems reduce on-site construction and commissioning requirements, helping operators execute projects more efficiently in remote environments and bring critical assets online faster.

"Standardization doesn't limit flexibility. It enables faster execution, lower lifecycle costs, and more predictable project outcomes."

Josh Wilkerson - EPIC Industrial Owner, President, and Director

Optimized architectures that leverage synchronous transfer allow customers to do more with less while maintaining the reliability, availability, and operational performance critical to compression and pipeline operations. Standardized designs also provide a scalable framework that can be replicated across facilities, enabling more consistent execution as midstream networks expand. Together, EPIC and Rockwell Automation have transformed what was once a highly customized engineering effort into a repeatable solution that delivers predictable outcomes for the oil and gas industry.

Published November 10, 2026

Topics: Optimize Production Packaged Solutions Oil & Gas Drives Motor Control
Subscribe to Rockwell Automation

Receive the latest news, thought leadership and information directly to your inbox.

Subscribe now

You may also be interested in

Loading
Loading
Loading
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Case Studies
  5. Chevron LeftChevron Left EPIC Industrial: From Packaged Power to Operational Value
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
CloseClose