Option button
Selects a mutually exclusive option in a group of options.
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Word wrap | WordWrap | Enable/disable the automatic word wrapping when the text is wider than the container. Ignored when the object width is automatic or when text abbreviation is set. | |
Text trimming | Elide | Text trimming mode. Insert three dots (...) in the indicated position when the text is too long for the available space. Ignored when the object width is automatic or when word wrap is set. | |
Checked | Checked | Interrupter status. To enable another interface object when the value is True, create a dynamic link between this property and the Enabled property of the object to be enabled. | |
Events
Modified value
- BrowseName
Provide Feedback