Element

BrowseName
Item
SuperType
Base UI object type(BaseUIObject)

Properties

Name
BrowseName
DataType
Description
Visible
Visible
Show/hide the window.
Enabled
Enabled
Enables/disables the interaction with the user (True = enabled; False = disabled).
Opacity
Opacity
Opacity level (0 = transparent).
Left margin
LeftMargin
(Only if Horizontal Alignment = Left or Center or Stretch) Distance between the left edge of the object and the left edge of its container.
Top margin
TopMargin
(Only if Vertical Alignment = Top or Center or Stretch) Distance between the top edge of the object and the top edge of its container.
Right margin
RightMargin
(Only if Horizontal Alignment = Right or Center or Stretch) Distance between the right edge of the object and the right edge of its container.
Bottom margin
BottomMargin
(Only if Vertical Alignment = Bottom or Center or Stretch) Distance between the bottom edge of the object and the bottom edge of its container.
Width
Width
Width of the window. It can assume values greater than or equal to zero. The Auto value sets the width equal to the width of the content (in this case, in the absence of content the object collapses).
Height
Height
Height of the window. It can assume values greater than or equal to zero. The Auto value sets the height equal to the height of the content (in this case, in the absence of content the object collapses).
Horizontal alignment
HorizontalAlignment
Alignment of the object on the horizontal axis. Left = the left side is positioned on the left side of the container, except for the left margin; Right = the right side is positioned on the right side of the container, except for the right margin; Center = the center of the object is positioned in the center of the container, except for the left and/or right margins; Stretch = object width equals container width, except for the left and/or right margins.
Vertical alignment
VerticalAlignment
Alignment of the object on the vertical axis. Top = the top side is positioned on the top side of the container, except for the top margin; Bottom = the bottom side is positioned on the bottom side of the container, except for the bottom margin; Center = the center of the object is positioned in the center of the container, except for the top and/or bottom margins; Stretch = object height equals container height, except for the top and/or bottom margins.
Rotation
Rotation
Rotation of the object around its center point. Positive values indicate clockwise arc degrees.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal