Navigation panel

Panel that contains other panels and automatically organizes them into navigable tabs.
BrowseName
NavigationPanel
SuperType
Container(Container)

Properties

Name
BrowseName
DataType
Description
Current panel
CurrentPanel
Node ID of the node of the panel displayed.
Tab position
TabPosition
Position of the navigation tabs on the y axis.
Panels
Panels
Collection of Panel objects to display.
Visible
Visible
(Inherited from Element)
Enabled
Enabled
(Inherited from Element)
Opacity
Opacity
(Inherited from Element)
Left margin
LeftMargin
(Inherited from Element)
Top margin
TopMargin
(Inherited from Element)
Right margin
RightMargin
(Inherited from Element)
Bottom margin
BottomMargin
(Inherited from Element)
Width
Width
(Inherited from Element)
Height
Height
(Inherited from Element)
Horizontal alignment
HorizontalAlignment
(Inherited from Element)
Vertical alignment
VerticalAlignment
(Inherited from Element)
Rotation
Rotation
(Inherited from Element)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.