Label

Visualizes a text.
BrowseName
Label
SuperType
Element(Item)

Properties

Name
BrowseName
DataType
Description
Text
Text
Text inserted and displayed.
Text horizontal alignment
TextHorizontalAlignment
Indicates where the text is positioned on the horizontal axis.
Text vertical alignment
TextVerticalAlignment
Indicates where the text is positioned on the vertical axis.
Word wrap
WordWrap
Enable/disable the automatic word wrapping when the text is wider than the container. Ignored when the object width is automatic or when text abbreviation is set.
Text trimming
Elide
Text trimming mode. Insert three dots (...) in the indicated position when the text is too long for the available space. Ignored when the object width is automatic or when word wrap is set.
Font family
FontFamily
Font family.
Font weight
FontWeight
Font weight.
Font italic
FontItalic
Enables/disables italics in the text.
Font size
FontSize
Font size.
Text color
TextColor
Color of the text to display.
Blink
Blink
Allows the object to periodically blink, ignored when the object is not visible.
Visible
Visible
(Inherited from Element)
Enabled
Enabled
(Inherited from Element)
Opacity
Opacity
(Inherited from Element)
Left margin
LeftMargin
(Inherited from Element)
Top margin
TopMargin
(Inherited from Element)
Right margin
RightMargin
(Inherited from Element)
Bottom margin
BottomMargin
(Inherited from Element)
Width
Width
(Inherited from Element)
Height
Height
(Inherited from Element)
Horizontal alignment
HorizontalAlignment
(Inherited from Element)
Vertical alignment
VerticalAlignment
(Inherited from Element)
Rotation
Rotation
(Inherited from Element)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.