Editable label

Display an editable text.
BrowseName
EditableLabel
SuperType
Element(Item)

Properties

Name
BrowseName
DataType
Description
Text
Text
Text to display and possibly changed by the user.
Text horizontal alignment
TextHorizontalAlignment
Indicates where the text is positioned on the horizontal axis.
Text vertical alignment
TextVerticalAlignment
Indicates where the text is positioned on the vertical axis.
Word wrap
WordWrap
Enable/disable the automatic word wrapping when the text is wider than the container. Ignored when the object width is automatic or when text abbreviation is set.
Text trimming
Elide
Text trimming mode. Insert three dots (...) in the indicated position when the text is too long for the available space. Ignored when the object width is automatic or when word wrap is set.
Font family
FontFamily
Font family.
Font weight
FontWeight
Font weight.
Font italic
FontItalic
Enables/disables italics in the text.
Font size
FontSize
Font size.
Text color
TextColor
Color of the text to display.
Border color
BorderColor
Color of the polygon border.
Editable
Editable
Enable/disable the change of the value directly in the chart.
Visible
Visible
(Inherited from Element)
Enabled
Enabled
(Inherited from Element)
Opacity
Opacity
(Inherited from Element)
Left margin
LeftMargin
(Inherited from Element)
Top margin
TopMargin
(Inherited from Element)
Right margin
RightMargin
(Inherited from Element)
Bottom margin
BottomMargin
(Inherited from Element)
Width
Width
(Inherited from Element)
Height
Height
(Inherited from Element)
Horizontal alignment
HorizontalAlignment
(Inherited from Element)
Vertical alignment
VerticalAlignment
(Inherited from Element)
Rotation
Rotation
(Inherited from Element)

Events

Modified text
BrowseName
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.