Combo box

Drop-down selection whose elements are obtained from a model of the project nodes or from one or more database tables.
BrowseName
ComboBox
SuperType
Element(Item)

Properties

Name
BrowseName
DataType
Description
Text
Text
(Only with Mode=Editable) Text of the written/selected element. Can be used to create customized logics (for example, create new nodes).
Model
Model
Reference to the information model or database from which to obtain the data.
Selected value
SelectedValue
Value of the property set in Path of the value selected when an element is selected at runtime.
Selected item
SelectedItem
Element selected when the object is initialized at runtime (if empty, it is initialized without selections). After initialization, this property displays the node corresponding to the selected element (access to the property is both read and write when the data are obtained from project nodes, read-only when obtained from a database).
UI selected item
UISelectedItem
UI selected value
UISelectedValue
Allow deselection
AllowDeselection
Display value path
DisplayValuePath
Attribute/property of the nodes or column of a database table whose value is to display in the list. When a value is not assigned, if the model is node-based, the BrowseName of the nodes is displayed; if the model is based on a database, the value of the first cell of each row is displayed, except for queries that further filter the values.
Selected value path
SelectedValuePath
Property with which to assign a value to the Value property selected at runtime when selecting an element.
Query
Query
Standard SQL query to filter the data of interest. You can use it to filter data from a database and to filter data obtained from a node-based model. In case of a node-based model, the SELECT * FROM Model part is mandatory, followed by the WHERE clause with which to indicate the search conditions - for example: SELECT * FROM Model WHERE Speed > 40
Mode
Mode
Mode of selection of the elements. Normal = selection with click; Normal with text search = selection with click or full typing of an existing element; Editable = selection with click or full typing of an existing or new element.
Font family
FontFamily
Font family.
Font weight
FontWeight
Font weight.
Font italic
FontItalic
Enables/disables italics in the text.
Font size
FontSize
Font size.
Text color
TextColor
Color of the text to display.
Sort order
SortOrder
Default sort order, ascending or descending, of the elements.
Order by
OrderBy
Attribute/property of the nodes or column of a table by which to sort the elements. Generally the same attribute/property or column from which the elements are obtained is set.
Visible
Visible
(Inherited from Element)
Enabled
Enabled
(Inherited from Element)
Opacity
Opacity
(Inherited from Element)
Left margin
LeftMargin
(Inherited from Element)
Top margin
TopMargin
(Inherited from Element)
Right margin
RightMargin
(Inherited from Element)
Bottom margin
BottomMargin
(Inherited from Element)
Width
Width
(Inherited from Element)
Height
Height
(Inherited from Element)
Horizontal alignment
HorizontalAlignment
(Inherited from Element)
Vertical alignment
VerticalAlignment
(Inherited from Element)
Rotation
Rotation
(Inherited from Element)

Methods

Refresh
BrowseName
Refresh

Events

Selection changed
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal