Advanced SVG Image
Displays an SVG Tiny 1.2 image and makes it possible to change the properties of individual parts of the image at design time or at runtime.
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Fill Mode | FillMode | Fill mode of the image object (Fit = resize the image keeping the original aspect ratio, Stretch = resize the image by fitting the aspect ratio to the area of the image object). | |
Hit test visible | HitTestVisible | True = intercept user clicks. False = does not intercept user clicks, which are instead passed to the underlying object, based on the order on the Z axis. | |
Colorization mode | ColorizationMode | Set the colorization mode which will be used when applying the selected color to the image. | |
SVG Element Properties | SVGElementProperties | Set the color of a part of the SVG file. | |
Provide Feedback