Objects and types

An
object
is an element that represents a physical or non-physical component in the project. A
type
is a model or template object for creating instances of an object.
Create objects from
Project view
or
Type view
. Any graphic object that you create in the default
UI
folder or a subfolder of the
UI
folder is automatically configured as a type. Types are available in
Type
view
in the
UI
folder.
Change the properties of an object or type instance to change the appearance and data values displayed for that instance at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.