Create an object type
Create an object type so that you can create instances of that type to show different values at runtime. Create a new type in
Type view
.When you create an object type, the original object from which you create the type becomes an instance of the new type.
- FromProjectview, drag an object into a folder inTypeview.
The new object appears in
Type view
and the object name is appended with "(type)". The new type also appears in the same folder in Project
view
. Provide Feedback