Loading

Lathes

Compartilhar:

EmailEmail
PrintPrint
  • Tipo: e-Learning
  • Tecnologia: Craft Skills
  • Categoria: Understand
E-Learning Course Catalog

Overview

This course provides instruction on the use of a lathe for turning and shaping metal workpieces, including how to use various cutting tools and grinders to produce precise shapes and finishes. Participants will be presented with information on how to operate and control an engine lathe, install and remove chucks and faceplates with cam locks, and perform alignment and centering procedures. This course will also cover how to perform rough and precision layouts of workpieces, and the correct procedures for sawing stock, straight and draw filing, sizing holes with hand reamers, tapping threads by hand, deburring parts, and removing broken studs. 


Prerequisites

There are no prerequisites for this course.

Who Should Attend

Maintenance Shop Equipment

Objectives

Make a right hand turning tool on a grinding machine.

Explain the function of the operator controls on an engine lathe.

Install and remove chucks and face plates with cam locks on an engine lathe.

Describe the steps required to rough center work in a 4-jaw chuck on an engine lathe.

Describe the steps required to face the end surfaces and shoulders of a work specimen on a lathe.

Describe the steps required to perform alignment of lathe centers.

Describe the steps required to perform alignment of lathe centers.

Describe the steps required to mount work pieces between centers on a lathe.

Describe the steps required to carry out straight turning between centers on a lathe.

Describe the steps required to knurl a work piece on a lathe.

Describe the steps required to do taper turning on a lathe using the tail stock off-set method.

Describe the steps required to do straight turning of a work specimen held in a chuck on an engine lathe.

Describe the steps required to perform precision centering work in a 4-jaw chuck on a lathe.

Describe the proper method to cut steep tapers and chamfers on a lathe.

Describe the steps required to perform drilling in a lathe.

Describe the steps required to execute machine reaming in a lathe.

Describe the steps required to do parting and grooving in a lathe.

Describe the steps required to grind a 60º threading tool.

Describe the steps required to cut external unified standard screw threads on a lathe.

Describe the steps required to grind a radius tool.

Describe the steps required to grind a round nose form tool.

Describe the steps required to perform radius and fillet turning on a lathe.

Describe the steps required to perform boring operations using a lathe.

Describe the steps required to cut internal unified standard screw threads using a lathe.

Describe the steps required to center drill work between centers using a lathe.

Describe the steps required to grind a right hand facing tool.

Describe the steps required to perform taper turning in a lathe with taper attachment.

Describe the steps required to mount, face and turn work on a mandrel.

Describe the steps required to reverse the jaws in a 4-jaw independent chuck.

Describe the steps required to change the jaws in a 3-jaw universal chuck.

Describe the steps required to reverse the jaws in a 3-jaw universal chuck with cap screw mounted jaws.

Describe the use of a steady rest.

Describe the steps required to straighten a shaft using a lathe.


Pronto para conversar com um Especialista em Inscrição de Treinamento?

Como adquirir

Para adquirir produtos de treinamento ou para saber mais sobre nossas soluções de treinamento, entre em contato com o escritório de vendas ou distribuidor local.

Como acessar

Para visualizar os cursos presenciais disponíveis oferecidos e para visualizar os cronogramas dos cursos atuais Portal de serviços de treinamento.

Como obter suporte

Precisa de ajuda com a seleção de curso, opções de estação de trabalho ou algo mais?

Enviar email para um Representante de Inscrição

textura de fundo gradiente cinza
  1. Chevron LeftChevron Left Página inicial da Rockwell Automation
  2. Chevron LeftChevron Left Sup...
  3. Chevron LeftChevron Left Serviços de treinamento de desenvolvimento de força de trabalho
  4. Chevron LeftChevron Left Assinaturas do treinamento Learning+
  5. Chevron LeftChevron Left Lathes
O conteúdo deste site foi traduzido usando inteligência artificial (IA) sem revisão nem edição humana. O conteúdo pode conter erros ou imprecisões e é fornecido “da forma como está” sem nenhum tipo de garantia. O texto oficial é a versão em inglês.