Loading
Overview

A Proactive Approach to Cyber Security

Compartilhar:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail

The Industrial Internet of Things is driving a level of increased connectivity that helps companies to improve their overall performance, but also comes with the potential for enterprise risk. With the potential for huge losses at stake, applying cyber security to industrial control systems means taking a holistic and proactive approach to managing that risk and protecting operations and intellectual property. As attacks become more sophisticated and pervasive, physical security is not enough; companies also need to adopt an industrial cyber security posture. Rockwell Automation brings strong expertise of the plant floor as well as expertise in cyber security to help our customers secure and maintain their infrastructure, protect their assets, and optimize their overall performance. Learn more at rok.auto/securityservices.

Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe
  1. Chevron LeftChevron Left Página inicial da Rockwell Automation
  2. Chevron LeftChevron Left Suporte
  3. Chevron LeftChevron Left Documentação
  4. Chevron LeftChevron Left A Proactive Approach to Cyber Security
O conteúdo deste site foi traduzido usando inteligência artificial (IA) sem revisão nem edição humana. O conteúdo pode conter erros ou imprecisões e é fornecido “da forma como está” sem nenhum tipo de garantia. O texto oficial é a versão em inglês.