UIPopulator NetLogic 만들기

모델 개체 속성을 기반으로 UI 요소를 자동으로 만드는 NetLogic을 만듭니다.
필수 구성 요소
기본 외부 코드 편집기를 설정합니다. 기본 코드 편집기 설정 항목을 참조하십시오.
  1. UIPopulator NetLogic을 만들려면
  2. 프로젝트 보기
    에서
    세로레이아웃1
    을 마우스 오른쪽 버튼으로 클릭하고
    새로 만들기
    런타임 NetLogic
    을 선택합니다.
  3. NetLogic 위로 마우스를 가져가서
    Edit
    을 선택하고
    UIPopulator
    을 입력합니다.
  4. NetLogic을 두 번 클릭합니다.
    외부 코드 편집기가 열립니다.
  5. 코드 편집기에서 기존 코드를 다음 코드로 바꿉니다.
    using System.Linq; using FTOptix.HMIProject; using FTOptix.UI; using UAManagedCore; using OpcUa = UAManagedCore.OpcUa; public class UIPopulator : FTOptix.NetLogic.BaseNetLogic { public override void Start() { // Get the Model variable of the ListBox modelObjectVariable = LogicObject.Get<IUAVariable>("ModelObject"); // Subscribe to the VariableChange event modelObjectVariable.VariableChange += ModelObjectVariable_VariableChange; // Build the UI based on the selected item BuildUI(modelObjectVariable.Value); } private void ModelObjectVariable_VariableChange(object sender, VariableChangeEventArgs e) { // Every time the ModelObject variable changes, rebuild the UI BuildUI(e.NewValue); } public override void Stop() { // Destroy the variable change event modelObjectVariable.VariableChange -= ModelObjectVariable_VariableChange; } private void BuildUI(NodeId modelObjectNodeId) { // Get the VerticalContainer that will hold the UI elements var verticalContainer = (ColumnLayout)Owner; // Get the ModelObject of the VerticalLayout from the NodeId var modelObject = InformationModel.Get(modelObjectNodeId); // Clear all the children of the VerticalContainer foreach (var child in verticalContainer.Children.OfType<Item>()) { child.Delete(); } // Create the UI elements based on the DataType of the children of the ModelObject foreach (var objectProperty in modelObject.Children.OfType<IUAVariable>()) { Item uiObject; if (objectProperty.DataType == OpcUa.DataTypes.Boolean) uiObject = MakeSwitch(objectProperty); else if (objectProperty.DataType == OpcUa.DataTypes.String) uiObject = MakeTextBox(objectProperty); else if (objectProperty.DataType == OpcUa.DataTypes.Int32) uiObject = MakeLinearGauge(objectProperty); else if (objectProperty.DataType == OpcUa.DataTypes.Float) uiObject = MakeCircularGauge(objectProperty); else if (objectProperty.DataType == FTOptix.Core.DataTypes.ResourceUri) uiObject = MakeImage(objectProperty); else uiObject = MakeTextBox(objectProperty); // Add the UI element to the VerticalContainer if (uiObject != null) verticalContainer.Add(uiObject); } } private static Panel MakeBaseContainer(IUAVariable variable) { // Create a Panel to hold the UI element var container = InformationModel.MakeObject<Panel>("ControlContainer"); container.Height = 50; container.HorizontalAlignment = HorizontalAlignment.Stretch; // Create a Label to show the name of the variable var label = InformationModel.MakeObject<Label>("Label"); label.VerticalAlignment = VerticalAlignment.Center; label.LeftMargin = 20; label.Text = variable.BrowseName; // Add the Label to the Panel container.Add(label); return container; } private static Item MakeSwitch(IUAVariable variable) { // Create a base container var container = MakeBaseContainer(variable); var mySwitch = InformationModel.MakeObject<Switch>("Switch"); mySwitch.HorizontalAlignment = HorizontalAlignment.Right; mySwitch.VerticalAlignment = VerticalAlignment.Center; mySwitch.RightMargin = 40; // Bind the Checked property of the Switch to the variable MakeDataBind(mySwitch.Children.Get<IUAVariable>("Checked"), variable); // Add the Switch to the container container.Add(mySwitch); return container; } private static Item MakeTextBox(IUAVariable variable) { // Create a base container var container = MakeBaseContainer(variable); var textBox = InformationModel.MakeObject<TextBox>("TextBox"); textBox.HorizontalAlignment = HorizontalAlignment.Right; textBox.VerticalAlignment = VerticalAlignment.Center; textBox.RightMargin = 40; // Bind the Text property of the TextBox to the variable MakeDataBind(textBox.Children.Get<IUAVariable>("Text"), variable); // Add the TextBox to the container container.Add(textBox); return container; } private static Item MakeCircularGauge(IUAVariable variable) { // Create a base container var container = MakeBaseContainer(variable); container.Height = 180; // Create a CircularGauge var circularGauge = InformationModel.MakeObject<CircularGauge>("CircularGauge"); circularGauge.Width = 140; circularGauge.HorizontalAlignment = HorizontalAlignment.Right; circularGauge.VerticalAlignment = VerticalAlignment.Stretch; circularGauge.RightMargin = 40; circularGauge.TopMargin = 20; // Bind the Value property of the CircularGauge to the variable MakeDataBind(circularGauge.Children.Get<IUAVariable>("Value"), variable); // Add the CircularGauge to the container container.Add(circularGauge); return container; } private static Item MakeLinearGauge(IUAVariable variable) { // Create a base container var container = MakeBaseContainer(variable); container.Height = 150; // Create a LinearGauge var linearGauge = InformationModel.MakeObject<LinearGauge>("LinearGauge"); linearGauge.Width = 140; linearGauge.Height = 35; linearGauge.HorizontalAlignment = HorizontalAlignment.Right; linearGauge.VerticalAlignment = VerticalAlignment.Center; linearGauge.RightMargin = 40; linearGauge.TopMargin = 20; // Bind the Value property of the LinearGauge to the variable MakeDataBind(linearGauge.Children.Get<IUAVariable>("Value"), variable); // Add the LinearGauge to the container container.Add(linearGauge); return container; } private static Item MakeImage(IUAVariable variable) { // Create the image object var image = InformationModel.MakeObject<Image>("Image"); image.HorizontalAlignment = HorizontalAlignment.Center; image.Width = 100; image.Height = 100; image.TopMargin = 20; image.BottomMargin = 20; // Set the path property of the image object image.Path = new FTOptix.Core.ResourceUri(variable.Value); return image; } private static void MakeDataBind(IUAVariable property, IUAVariable targetVariable) { // Set the DynamicLink to a variable as ReadWrite property.SetDynamicLink(targetVariable, FTOptix.CoreBase.DynamicLinkMode.ReadWrite); } private IUAVariable modelObjectVariable; }
  6. 코드를 저장합니다.
의견을 작성 부탁드립니다.
이 자료에 대한 문의사항이나 요청사항이 있습니까? 여기에 요청사항을 작성 부탁드립니다.
Normal