Loading

Field Devices

Condividi:

EmailEmail
PrintPrint
  • Tipo: e-Learning
  • Tecnologia: Craft Skills
  • Categoria: Understand
E-Learning Course Catalog

Overview

This course focuses on the operation, maintenance, and repair of oil and gas ignition systems, pulverizers, and coal feeders commonly used in power generation. The course also presents the identification of the major components of these systems and understand their functions along with how to troubleshoot and repair the devices.


Prerequisites

There are no prerequisites for this course.

Who Should Attend

Instrumentation & Control Technician

Objectives

   Identify and state the function of the major components of an oil/gas ignitor.

   Describe the basic steps required for troubleshooting and repairing oil/gas ignitors.

   Identify major components of warm-up oil guns.

   Describe the basic steps required to troubleshoot and repair of instrumentation devices on warm-up oil guns.

   Identify and state the function of the major instrument components on a pulverizer.

   Describe the basic steps required to troubleshoot and repair instrumentation devices on a coal pulverizer.

   Identify and state the function of the major instrumentation components on a coal feeder.

   Describe the basic steps required to troubleshoot and repair coal feeder instrumentation.

   Describe the basic steps required to troubleshoot and repair the coal pulverizer inerting system.

   Identify major components of a flame scanning system.

   Explain troubleshooting and repair procedures for flame scanning systems.

   Describe the basic steps required to troubleshoot and repairing auxiliary air damper controls.

   Describe the basic steps required to troubleshoot and repair insert/retract mechanisms.

   Describe the basic steps required to troubleshoot and repair impeller drives.

   Describe the basic steps required for the troubleshooting and repair of oil and gas valve controls.

   Identify the major components of oil guns.

   Describe the basic steps required to troubleshoot and repair of instrumentation devices on oil guns.


Siete pronti per parlare con uno specialista addetto all’iscrizione ai corsi di formazione?

Come acquistare

Per acquistare prodotti per la formazione o per ottenere ulteriori informazioni sulle soluzioni di formazione, contattate l'ufficio commerciale o il distributore locale.

Come ottenere assistenza

Avete bisogno di aiuto con la scelta dei corsi, le proposte della stazione di lavoro o altro?
Contattate i servizi di formazione.

sfondo trama grigio gradiente
  1. Chevron LeftChevron Left Home Rockwell Automation
  2. Chevron LeftChevron Left Ass...
  3. Chevron LeftChevron Left Servizi per la formazione professionale del personale
  4. Chevron LeftChevron Left Abbonamenti ai corsi di formazione Learning+
  5. Chevron LeftChevron Left Field Devices
I testi di questo sito sono stati tradotti utilizzando l'intelligenza artificiale (AI) senza revisione o modifica da parte di esseri umani. I testi possono contenere errori o imprecisioni e sono forniti “così come sono” senza alcun tipo di garanzia. Il testo ufficiale è la versione inglese del contenuto.
Aggiorna le tue preferenze sui cookie per continuare.
Questa funzionalità richiede i cookie per migliorare la tua esperienza. Ti preghiamo di aggiornare le tue preferenze per consentire questi cookie: