Loading
Case Study | Packaging
Recent ActivityRecent Activity

Packaging Company Improves Food Sortation System

Arena® Simulation Software helps determine best instrumentation alternative.

Condividi:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
apples being sorted on four sorting conveyor belts

Challenge

Analyze multiple scenarios to increase sortation system’s performance

Solutions

A model was built to represent the sortation system, input conveyor, and exit conveyor.

Results

  • Implementation of a combined sensor and timer based release system
  • The combination alternative has proven 95% to 98% effective in meeting the system’s objective of an enhanced packaging process flow

Background

A large packaging system company in Glasgow, Kentucky, produces continuous, plastic-chain, curving conveyors used primarily for food production. In addition to conveyor systems this packaging company also produces a complete line of transfers for handling products at the start and end points of the conveyor. Conveyor systems running an optimal packaging process flow is imperative to the product’s success. 

Challenge

A food sortation system developed by this packaging manufacturer was designed to take a random stream of frozen pies from a wide belt conveyor and manipulate the packaging process flow to generate a single file output- without pies colliding during the process. The sortation system, already installed at a client’s site, was not meeting three key performance criteria: 

  1. No pie collisions 
  2. Meet a maximum input rate of 50 pies per minute
  3. Create a 17-inch distance between pie centers upon exit

Solution

Since the system had been installed already and was in operation on a daily basis, the Rockwell Automation Arena consulting team was called to build a model using Arena packaging optimization software. Simulating a packaging process flow model to vary the current system would allow the packaging manufacturer to conduct analysis without disturbing the actual system or building costly prototypes. 

The model was built to represent the sortation system, input conveyor, and exit conveyor. The Arena model was constructed to allow selection between two types of release mechanisms, one which was timer-based and another which was sensor-based. An animation of the packaging prcoess flow was developed in Arena so that analysts could observe the movement of pies and and keep track of vital statistics during the course of the run. 

Results

The packaging optimization model was used to test a strictly sensor base system, a timer-based system, and a combination of the two. the third option was selected because, during simulation runs, the sensor-based system increased the number of high velocity pie collisions that occurred, and the timer-based system built up too many queues inside the sortation system. The combination alternatively brought together the best of the first two options and has proven 95% to 98% effective in meeting the system objectives. 

Pubblicato 31 luglio 2014

Argomenti: Food & Beverage Arena Simulation Software Packaging Simulation Software Food and Beverage Simulation Software

Ready to Order Your Software?

Ordering Options
Software SubscriptionsSoftware Subscriptions
Ordering Options

One stop shopping for software and subscription services.

Explore Our Ordering Options
Talk to a Consultant
DistributorDistributor
Talk to a Consultant

Work with your local Rockwell Automation sales consultant to discuss your software requirements.

Contact Us

Recommended For You

Loading
  1. Chevron LeftChevron Left Home Rockwell Automation
  2. Chevron LeftChevron Left Pro...
  3. Chevron LeftChevron Left Sof...
  4. Chevron LeftChevron Left Software di simulazione Arena
  5. Chevron LeftChevron Left Arena Simulation Software Case Studies
  6. Chevron LeftChevron Left Packaging Company Improves Sortation System
I testi di questo sito sono stati tradotti utilizzando l'intelligenza artificiale (AI) senza revisione o modifica da parte di esseri umani. I testi possono contenere errori o imprecisioni e sono forniti “così come sono” senza alcun tipo di garanzia. Il testo ufficiale è la versione inglese del contenuto.
Aggiorna le tue preferenze sui cookie per continuare.
Questa funzionalità richiede i cookie per migliorare la tua esperienza. Ti preghiamo di aggiornare le tue preferenze per consentire questi cookie: