Scroll view example

Use this object to provide a panel that includes scroll bars, so that it can contain content larger than the panel itself.
MANCIA:
Scroll view
supports:
  • Touch and multitouch gestures, such as pan or pinch-to-zoom.
  • Keyboard and mouse operation, such as the
    Ctrl
    Scroll wheel
    combination to zoom-in or zoom-out.
Scroll view example

Use case

Display overview information, drawings, or other items that are larger than the main application container.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.