Configure a Navigation panel
Configure a
Navigation panel
by referencing Panel objects as tabs.- InProject view, create or select aNavigation panelobject.
- CreatePaneltypes that you want to reference as tabs in theNavigation panel.
- SelectNavigation panel. InPropertiesadd tabs by selectingnext toPanels.
- Create dynamic links betweenPanelproperties andPaneltypes.For more information about dynamic links, see Create dynamic links.
- (optional) Change tab titles by editing theTitleproperty values.
- (optional) Add images to tabs by editing theImage pathproperty values.
Fornire un feedback