Create an OPC UA method

In
FactoryTalk Optix Studio
, you can create an OPC UA method and then edit its code in an external code editor.
Prerequisites
Set the default external code editor. See Set the default code editor.
  1. In the
    Project view
    pane, right-click
    NetLogic
    and select
    New
    Runtime NetLogic
    .
  2. Right-click the
    RuntimeNetLogic
    that you created and select
    New
    Method
    .
    The external code editor opens. The following code is added in the NetLogic:
    [ExportMethod] public void MethodName() { }
  3. (Optional) Rename the method in C#.
Develop the code of the method.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.
Normal