Develop a login page

Develop a login page that handles correct and incorrect login attempts.
Application example
SUGGERIMENTO:
You can download a sample project from:
ExampleApplication-LoginPage.zip
Prerequisites:
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.
Normal