Integrate the application interface with the script
    Make the button trigger the label text change when you select the button.
- Define a mouse click event for the button:- In theProject viewpane, selectButton1.
- In theEventspane, next toMouseClickEvent, selectand select . 
 
- Create a dynamic link between thelabelNodeIdproperty andLabel1.For more information about dynamic links, see Create dynamic links.
Fornire un feedback