API to write log messages

Use C# APIs to generate log messages.
The APIs are supplied by the static
Log
C# class.
SUGGERIMENTO: If the log messages are generated by
FactoryTalk Optix Studio
at design time or by a
FTOptixApplication
at runtime on a connected target, you can display the log messages in the
FactoryTalk Optix Studio
Log
pane. You can also display the message category in the
Module
column of the
Log
pane.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.
Normal