Develop a constrained linear gauge

Develop an interface that enables you to change the current value, max value, and minimum value of a variable.
NOTA:
Download the sample
FactoryTalk Optix Studio
project:
ExampleApplication-ConstrainedLinearGauge.zip
Prerequisites:
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.
Normal