Create a linear gauge
Create a linear gauge that shows the temperature.
- In thePropertiespane, right-clickMainWindow (type)and select .
- In thePropertiespane, set theEditablevariable value toFalse.
- Create a variable:
- In thePropertiespane, at the top, selectand selectAnalog variable.
- Create a complex dynamic link between theAnalogVariable1property and the actualAnalogVariable1variable by using binding mode.
- DynamicLink
- Binding mode between Source and Parent engineering unit
- Set Parent localized engineering unit.
- Create a dynamic link between theLow limitproperty and
- Create a dynamic link between theHigh limitproperty and
- Set theConstrainproperty value toTrue.
For more information about dynamic links, see Create dynamic links. - Link the variable alias:
- In thePropertiespane, create a dynamic link between theValueproperty and .
- Create a dynamic link between theMinimum valueproperty and .
- Create a dynamic link between theMaximum valueproperty and .
For more information about dynamic links, see Create dynamic links.
Fornire un feedback