Develop a solution that samples and stores data based on value change

Create an application that samples the value of a variable on the value change and stores that data in an embedded database.
Application example
NOTA:
Download the sample
FactoryTalk Optix Studio
project:
ExampleApplication-SampleStoreDataValueChange.zip
Prerequisites:
  1. Create a data logger with an embedded database that monitors the value change of the variable. See Add a data logger.
  2. Arrange the interface elements.
  3. Save the project.
Application design example
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.