Create a list of motors

Create a list box populated with motor objects.
  1. In the
    Project view
    pane, right-click
    MainWindow (type)
    and select
    New
    Data controls
    List box
    .
  2. Hover-over the list box, select
    Edit
    , and enter
    MotorListBox
    .
  3. In the
    Properties
    pane, create a dynamic link between the
    Model
    property and
    ProjectName
    Model
    MotorObjects
    For more information about dynamic links, see Create dynamic links.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.