VIDEO: Planetary Gearbox Has Less Than 1 Arcminute Backlash

At the 2017 Automation Fair® event, Eugene Detke from Apex Dynamics Inc. demonstrates the new AP and AH series, a carbon steel planetary gearbox with less than 1 arcminute backlash in a single stage and a double stage, and also the capability of up to 14,000 Nm torque. Delivery of standard products is guaranteed within two weeks or it’s free.

View the video now.

 

The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Putman Media, Inc.

The JOURNAL

Check Out the February Issue

The JOURNAL from Rockwell Automation and Our PartnerNetwork™ is a bimonthly magazine, published by Putman Media, Inc., designed to educate engineers about leading-edge industrial automation methods, trends and technologies.