How to Reduce Mechanical Resonance Issues and Improve Drive Performance

How to Reduce Mechanical Resonance

Low-voltage AC drives with advanced analytics can help cut costs by detecting and mitigating mechanical resonance issues, so machines run more efficiently.

It can be a scary moment on the plant floor: A machine starts shrieking and shaking so violently, you think it might break.

This type of incident can result from mechanical resonances caused by a load attached to a motor. Many design factors attribute to the resonances, such as physical size, material selection and installation procedures. And while workers usually can make a control adjustment to resume production, resonance issues have lasting consequences on your machines and your business.

In the past, the typical adjustment to resolve the resonance either degraded performance or resulted in wasted energy.  

New low-voltage AC drives with adaptive tuning can help better combat resonance issues, so performance is better and you spend less. During production, the drive identifies the problem and applies the correct solution, resulting in a higher-performing machine that accounts for machine variations.

Think of these smart drives like guards. They keep a vigilant watch of your application for undesirable resonance. If they see something wrong, they can sound the alarm or even attack the issue on their own. And by helping you win the war against resonance, the drives can help you stay up and running longer while helping to reduce your repair and energy costs.

Protect the Machine’s Potential

Resonances result from design decisions that may or may not be modeled by the designer. Known design decisions include the load shape, material selection, dimensions and physical size. Unknown design decisions include tolerances, assembly processes and motor characteristics.

The resonances may change over time because of normal machine wear and tear. This can include applications that use shaft extensions or large loads like winders.

The previous approach to resolving resonances is to detune the regulator gains. This can stop a machine from shrieking and shaking, but it can also decrease the machine’s performance. Over time, this hurts your throughput and slows your reaction time to issues.

An AC drive with adaptive tuning uses advanced analytics to continually look for and detect different types of resonance. The drive can alert operators of issues in real time, so they can act quickly.

In more advanced configurations, the drive can use special filters to mitigate resonance instead of detuning the controller.

This allows you to maintain a high level of performance. Based on load characteristics, we’ve seen two- to four-times-higher performance when using adaptive tuning.

Also, AC drives with adaptive tuning allow you to monitor resonance over time and schedule repairs, if conditions warrant. This can help you work smarter by addressing issues proactively and during scheduled maintenance windows, rather than abruptly in the middle of production.

Learn more about drives with adaptive tuning.

 

 

 

 

 

The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Putman Media, Inc.

Contact

Rockwell Automation and our partners offer exceptional knowledge to help design, implement, and support your automation investment.

Latest News

Subscribe to Rockwell Automation and receive the latest news and information directly to your inbox.